ESXP2G001EN-Trans-05

Recommended Time Accuracy

The time criticality of an application defines the recommended time accuracy of data logged for the application to achieve its intended output.

The overall time accuracy level of a digital system will be derived both from the individual performance of the connected product timestamp and by the synchronization of system components to a single, reliable, and accurate time reference.

Applications Time Criticality Recommended Time Accuracy [+/-] Minimum Required Time Accuracy [+/-]
Advanced Protection and Automation

High

1 ms

10 ms

Arc Flash Protection

High

1 ms

10 ms

Asset Performance

Low

1 s

10 s

Backup Power Testing

Medium

10 ms

100 ms

Circuit Breaker Settings Monitoring

Low

1 s

10 s

Capacity Management

Low

1 s

10 s

Continuous Thermal Monitoring

Low

1 min*

5 min*

Cost Allocation

Low

1 s

10 s

Electrical Asset Life Cycle Management

Low

1 min

5 min

Electrical Distribution Monitoring and Alarming

Medium

10 ms

1 s

Energy Benchmarking

Low

1 s

10 s

Energy Efficiency Compliance

Low

1 s

10 s

Energy Modeling and Verification

Low

1 s

10 s

Energy Monitoring

Low

1 s

10 s

Energy Performance

Low

1 s

10 s

Greenhouse Gas Reporting

Low

1 s

10 s

Guided Procedures Through Extended Reality

Low

1 s

10 s

Insulation Monitoring

Low

1 s

10 s

Microgrid

Medium

10 ms

100 ms

Operator Training Simulation*

High

1 ms

10 ms

Power Event Analysis

High

1 ms

10 ms

Power Factor Correction

Low

1 s

10 s

Power Quality Correction

Low

1 s

10 s

Power Quality Monitoring and Compliance

Medium

10 ms

100 ms

Power Source and Load Control

Medium

10 ms

100 ms

Simulate Before Operate*

High

1 ms

10 ms

Utility Bill Verification

Low

1 s

10 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?