990-91379H-001

Perform a Parallel Battery SPoT Mode Test in a Parallel UPS System

NOTICE
Risk of load drop
The load is not supported by the UPSs during a Battery SPoT mode test. Shut down any connected load or ensure alternative supply for the load before starting a Battery SPoT mode test.
Failure to follow these instructions can result in equipment damage.
NOTICE
risk of equipment damage
  • Batteries will be discharged to the low DC warning level and this will result in a short battery runtime after the test until the batteries are fully recharged.
  • Repeated battery testing or calibration can affect the service life of the battery.
Failure to follow these instructions can result in equipment damage.
NOTE: The Parallel battery SPoT mode test is only legally allowed to perform in some countries/areas. Please refer to local/national legislation.
NOTE: The parallel system must be configured with common battery only. Parallel battery SPoT mode is not applicable for a parallel UPS system with individual battery banks for the UPSs.

Prerequisites for each UPS in the parallel system:

  • All UPSs in the parallel system must have the same power rating and the same available power

  • UOB must be open

  • The UPS operation mode for each UPS in the parallel system must be Requested static bypass

  • The system operation mode for the parallel system must be Requested static bypass

  • The battery disconnect device(s) BB must be closed

  • There must be no detected surveillance faults

  • SSIB must be closed

  • The output voltage and frequency must be within the predefined limits

This feature performs a battery discharge test without the need for a load bank. During the battery SPoT mode test, the inverter is turned ON while the parallel UPS system is in requested static bypass. During the test, the parallel UPS system performs a battery runtime calibration test and adjusts the estimated runtime accordingly.

The output power can be manually adjusted from 0 to 100% load to be as close as possible to the operating conditions.

The test stops when the battery voltage has reached its shutdown level, or when the predefined discharge level has been reached.

NOTE: Parallel battery SPoT mode must be enabled by Schneider Electric during service configuration before this test is available.
  1. From the home screen on the display select Tests > Parallel battery SPoT mode.
  2. On page 1 of the menu for Parallel battery SPoT mode, verify that the prerequisites for performing a test is met and confirm that the load is powered if UOB is open during this procedure. Tap the arrow symbol to go to the next page.
  3. On page 2, follow the listed checklist. Tap the arrow symbol to go to the next page.
  4. On page 3, set the battery discharge level and the output power level. Tap the arrow symbol to go to the next page.
  5. On page 4, tap Start parallel battery SPoT mode to start the test.
    NOTE: If you wish to manually stop the test, tap Abort parallel battery SPoT mode.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?