990-91379C-001

Configure the Output

NOTE: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > Output .
    1. Set the AC voltage ph-ph to 380VAC, 400VAC, 415VAC, 440VAC, or 480VAC depending on your configuration.
    2. Set the Frequency to 50Hz ±1.0, 50Hz ±3.0, 50Hz ±10.0, 60Hz ±1.0, 60Hz ±3.0, or 60Hz ±10.0 depending on your configuration.
    3. Tap OK to save your settings and tap the arrow symbol to go to the next page.
    4. Set the Bypass and output tolerance (%). The bypass and output tolerance range is +3% to +10%, default is +10%.
    5. Set the Voltage compensation (%). The output voltage of the UPS can be adjusted up to ±3% to compensate for different cable lengths. Default is 0%.
    6. Set the Overload threshold (%). The overload range is 0% to 100%, default is 75%.
    7. Set the Transformer voltage compensation (%). The transformer voltage compensation range is 0% to 3%, default is 0%. See Output Transformer Voltage Compensation for more details and Configure the UPS Input for configuring that an output transformer is present.
    8. Tap OK to save your settings.
QR code for this page

Was this helpful?