990-91379E-001

Start Up and Add UPS to a Running Parallel System

Use this procedure to start up a UPS and add it to a running parallel system.

NOTE: Only operate a breaker when the associated breaker indicator lamp is illuminated.
  1. On this UPS, close the unit input breaker UIB (if open).
    The display turns on. The rebooting sequence lasts approximately 3 minutes.
  2. Select Control > Guided sequences > Start up a UPS in a parallel system, and follow the steps which appear on the display.
  3. Generic start-up procedure:
    NOTE: The following are generic start-up procedures. Always follow the steps of the Guided sequences which are specific to your system.
    1. Close the static switch input breaker SSIB (if present) for this UPS.
    2. Close the bypass backfeed breaker BF2 (if present) for this UPS.
    3. Close the battery breaker(s) for this UPS.
    4. Close the unit output breaker UOB for this UPS.
    5. On this UPS, select Control > Inverter > Inverter on or press the inverter ON button (hold for five seconds) on the system level controller.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?