Overview of User Interface
Display
Overview of the Home Screen
- 
                        
Home button - tap this button on any screen to return to the home screen.
 - 
                        
Main menu button - tap this button on any screen to access the menus.
 - 
                        
Mimic diagram button - tap this button on any screen to access the mimic diagram.
 - 
                        
Alarm status symbol - tap this button on any screen to access the active alarms log.
 
You can tap on the output or battery fields on the home screen to go directly to the detailed measurement pages.
Mimic Diagram
The mimic diagram will adapt to your system configuration – the mimic diagrams shown here are just examples.
The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.
In mimic diagrams for parallel systems, tap on the gray UPS to see the mimic diagram on UPS level.
Alarm Status Symbol
The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.
| Green: No alarms present in the UPS system. | |
| Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log. | |
| Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log. | |
| Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log. | 
Menu Tree
Main Menu
- 
                        
Status – see Submenus for Status.
 - 
                        
Logs – see View the Logs.
 - 
                        
Control – see Submenus for Control.
 - 
                        
Configuration – see Submenus for Configuration.
 - 
                        
Maintenance – see Submenus for Maintenance.
 - 
                        
Statistics – see Submenus for Statistics.
 - 
                        
About – see Submenus for About.
 - 
                        
Logout – see Change the Password.
 - 
                        
Flag button – see Set the Display Language.
 
Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.
Submenus for Status
- 
                        
Status – see View the System Status Information.
- 
                              
Input
 - 
                              
Output
 - 
                              
Bypass
 - 
                              
Battery
 - 
                              
Temperature
 - 
                              
Power modules
 - 
                              
Peak shaving
 - 
                              
Parallel*
 
 - 
                              
 
Submenus for Control
- 
                        
Control*
- 
                                 
Operation mode
- 
                                       
Transfer to bypass operation – see Transfer the UPS from Normal Operation to Static Bypass Operation.
 - 
                                       
Transfer to normal operation – see Transfer the UPS from Static Bypass Operation to Normal Operation.
 
 - 
                                       
 - 
                                 
Inverter
- 
                                       
Inverter on – see Turn the Inverter ON.
 - 
                                       
Inverter off – see Turn the Inverter OFF.
 
 - 
                                       
 - 
                                 
Charger – see Set the Charger Mode.
- 
                                       
Float
 - 
                                       
Boost
 - 
                                       
Equalization
 
 - 
                                       
 - 
                                 
Guided sequences
- 
                                       
Start up UPS system – see Start Up the UPS System from Maintenance Bypass Operation.
 - 
                                       
Shut down UPS system – see Shut Down the UPS System into Maintenance Bypass Operation.
 - 
                                       
Start up a UPS in a parallel system – see Start Up and Add UPS to a Running Parallel System.
 - 
                                       
Shut down UPS in a parallel system – see Isolate a Single UPS in the Parallel System.
 
 - 
                                       
 
 - 
                                 
 
Submenus for Configuration
- 
                        
Configuration*
- 
                              
UPS – see Configure the UPS Input.
 - 
                              
Output – see Configure the Output.
 - 
                              
Battery – see Configure the Battery Solution.
- 
                                       
Standard
- 
                                                
General settings
 
 - 
                                                
 - 
                                       
Custom
- 
                                                
General settings
 - 
                                                
Specific settings
 
 - 
                                                
 
 - 
                                       
 - 
                              
High efficiency – see Configure High Efficiency Mode.
- 
                                       
Schedule
 
 - 
                                       
 - 
                              
Grid interactive UPS – see View Configuration for Prioritizing Battery Operation When Input Contact is Activated and Enable Peak Shaving Mode.
- 
                                       
Protected Modbus
 
 - 
                                       
 - 
                              
Breakers – see Configure the Disconnect Devices.
 - 
                              
Contacts and relays
- 
                                       
Input contact – see Configure the Input Contacts.
 - 
                                       
Output contact – see Configure the Output Relays.
 
 - 
                                       
 - 
                              
Network – see Configure the Network.
- 
                                       
Integrated NMC
- 
                                             
IPV4
 - 
                                             
IPV6
 
 - 
                                             
 - 
                                       
Optional NMC
- 
                                             
IPV4
 - 
                                             
IPV6
 
 - 
                                             
 
 - 
                                       
 - 
                              
Modbus – see Configure the Modbus.
- 
                                       
Integrated NMC
- 
                                             
IPV4
 - 
                                             
IPV6
 
 - 
                                             
 - 
                                       
Optional NMC
- 
                                             
IPV4
 - 
                                             
IPV6
 
 - 
                                             
 
 - 
                                       
 - 
                              
General
- 
                                       
UPS name – see Set the UPS Name.
 - 
                                       
Date and time – see Set the Date and Time.
 - 
                                       
Display – see Configure the Display Preferences.
 - 
                                       
System
 - 
                                       
Reboot display
 
 - 
                                       
 - 
                              
Reminder – see Configure the Air Filter Reminder.
 - 
                              
Save/restore – see Save the UPS Settings on a USB Device and Restore the UPS Settings from a USB Device.
 - 
                              
Update status
 
 - 
                              
 
Submenus for Maintenance
- 
                        
Maintenance
- 
                                 
Buzzer – see Tests.
 - 
                                 
Status LEDs – see Tests.
 - 
                                 
Breaker lamp – see Tests.
 - 
                                 
Battery* – see Start a Battery Test and Stop a Battery Test.
 - 
                                 
Runtime calibration* – see Start a Runtime Calibration Test and Stop a Runtime Calibration Test.
 - 
                                 
Battery replacement*
 - 
                                 
Battery SPoT mode* – see Perform a Battery SPoT Mode Test in a Single UPS System.
 - 
                                 
Parallel battery SPoT mode* – see Perform a Parallel Battery SPoT Mode Test in a Parallel UPS System.
 - 
                                 
UPS report* – see Export UPS Report to a USB Device.
 
 - 
                                 
 
Submenus for Statistics
- 
                        
Statistics
- 
                                 
Electricity savings
- 
                                          
Settings
 - 
                                          
Simulation
 
 - 
                                          
 
 - 
                                 
 
Submenus for About
- 
                        
About
- 
                                 
UPS
 - 
                                 
Display
 - 
                                 
Integrated Network Management Card (NMC)
 - 
                                 
Optional Network Management Card (NMC)
 
 -