990-91379H-001

Important Safety Instructions — SAVE THESE INSTRUCTIONS

Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.

The addition of this symbol to a “Danger” or “Warning” safety message indicates that an electrical hazard exists which will result in personal injury if the instructions are not followed.

This is the safety alert symbol. It is used to alert you to potential personal injury hazards. Obey all safety messages with this symbol to avoid possible injury or death.

DANGER
DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
WARNING
WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
NOTICE is used to address practices not related to physical injury. The safety alert symbol shall not be used with this type of safety message.
Failure to follow these instructions can result in equipment damage.

Please Note

Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.

A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.

Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.

The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040-1, section 3.102).

FCC Statement

NOTE: This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful interference in which case the user will be required to correct the interference at his own expense.

Any changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

Electromagnetic Compatibility

NOTICE
Risk of electromagnetic disturbance
This is a product category C2 UPS product. In a residential environment, this product may cause radio inference, in which case the user may be required to take additional measures.
Failure to follow these instructions can result in equipment damage.

Safety Precautions

DANGER
hazard of electrical shock, explosion or arc flash
All safety instructions in this document must be read, understood and followed.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electrical shock, explosion or arc flash
After the UPS system has been electrically wired, do not start up the system. Start-up must only be performed by Schneider Electric.
Failure to follow these instructions will result in death or serious injury.
CAUTION
Risk of hot surface
The outer plates of the cabinet can exceed temperatures of 65 °C (149 °F) at 50 °C (122 °F) ambient room temperature, if the air filter(s) in the front door is clogged. Replace the air filter regularly as described in the UPS operation manual.
Failure to follow these instructions can result in injury or equipment damage.

ENERGY STAR Qualification


Select models are ENERGY STAR® qualified.
For more information on your specific model go to www.se.com.

Cybersecurity and Physical Security Recommendations

Install the Product in a Secure Location

Custodians should secure products from unauthorized physical access.

  • Access should be restricted to those who require access to maintain the product.

  • Restricted areas should be clearly marked for authorized personnel only.

  • Restricted areas should be secured by locked doors.

  • Access to the restricted areas should produce a physical or electronic audit trail.

Secure Access to the User Interface and Communication Ports of the Product

Install the product in a rack or cage that can be locked with a suitable key, or other physical methods. This will prevent access to the user interface and the physical communication ports of the product.

Description of Risk

Attackers with physical access to the product can access the equipment without authorization.

Recommendations

Physical security must be in place to control physical access to restricted areas and facilities containing the product. The product should be located under lock and key or protected by physical restraints that prevent unauthorized access or removal from restricted areas. Access to areas containing the product should only be granted to personnel who require access based on their job function.

Restricted areas should display signs that clearly indicate access is for authorized personnel only. Facilities containing the product should give minimum indication of their purpose, with no obvious signs identifying the presence of related functions.

Physical access control devices, such as key card readers, doors and cabinet locks, should be tested prior to use and on a periodic basis (e.g. annually). Resource custodians should produce physical or electronic audit trails to record all personnel's physical access to restricted areas for security incident investigation. Inventory of who has physical access to control devices should be regularly reviewed, and any inappropriate access identified during the review should be promptly removed.

Firmware Updates

Schneider Electric strongly recommends that you review the security bulletins that relate to your Schneider Electric product.

For information on new and updated security bulletins, visit the Schneider Electric Security Bulletins web page.

Cybersecurity and Network Management Cards

NOTE: Schneider Electric adheres to industry best practices in the development and implementation of embedded components of Schneider Electric Network Management Cards, which enable the devices to function remotely over the network. This includes a "Defense-in-Depth" approach to secure the connected products. You can find the Security Handbook for the different network management cards on the Schneider Electric website. The Security Handbook describes security features and options for the appliance.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.