990-91379G-001

Configure the Disconnect Devices

NOTE: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > Breakers.
  2. Tap the different disconnect devices in the mimic diagram to configure which disconnect devices are present in the UPS system. Square with a means that the disconnect device is present, empty square means that the disconnect device is not present. BF2 presence can only be configured by Schneider Electric Service.
    NOTE: The UPS can monitor up to four battery disconnect devices in a battery solution. The mimic diagram only shows one battery disconnect device BB even if more battery disconnect devices have been connected and configured for monitoring. If one or more of the monitored battery disconnect devices are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery disconnect devices are in the open position, the BB on the mimic diagram will show as open.
  3. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?