Position the UPS
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Perform one
of the following once the UPS is in its final position:
Failure to follow these instructions will result in death or serious injury.
|
- Push the UPS into final position.
- Reinstall the front transportation bracket (870-32577) on the UPS.
- Perform one of the following:
- Mount the front transportation bracket to the floor. Use appropriate hardware for the floor type.
- Lower the front and rear leveling feet on the UPS with a wrench
until they connect with the floor. The casters must not have contact
with the floor. Use a bubble-leveler to check that the UPS is level.
NOTICE Risk of equipment damageDo not move the cabinet after the leveling feet have been lowered.Failure to follow these instructions can result in equipment damage.NOTICE Risk of equipment damageInstall the front transportation bracket to avoid the UPS overheating from circulating hot air from the rear outlets. The front transportation bracket blocks the hot air backflow.Failure to follow these instructions can result in equipment damage.
DANGER