990-91380K-001

Prepare for HRG Earthing System

  1. Remove the two preconnected cables that connect the E terminal on the bonding contactor to the ground busbar. Discard the cables.
  2. Connect an external impedance between the E terminal on the bonding contactor and the ground busbar according to NEC article 250.36.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?