990-91380K-001

Connect Power Cables in the UPS in System up to 45 kAIC/kA Icw

NOTE: If a backfeed kit (GVLOPT003 or GVLOPT004) is part of your installation, the backfeed kit must be installed before the power cables are connected in the UPS. Follow the installation manual provided with the backfeed kit.
NOTE: If a Lithium-ion battery control breaker kit (GVLOPT005) is part of your installation, the Lithium-ion battery control breaker kit must be installed before the power cables are connected in the UPS. Follow the installation manual provided with the Lithium-ion battery control breaker kit.
  1. Remove the transparent plastic protectors (marked (A) on the illustration) from the busbars. If present, remove the plastic box (marked (B) on the illustration) from the cabling field for easier access. Save all parts for reinstallation after cable connection.
    NOTE: On newer UPS models, the box (marked (C) on the illustration) is integrated in the inner door of the UPS instead of being a separate part. The integrated box must not be removed from the inner door.

    Front View of the UPS Model with Separate Plastic Box

    Front View of the UPS Model with the Box Integrated in the Inner Door

  2. Only for dual mains: Remove the single mains busbars.
    NOTE: Save the three single mains busbars. They are needed for testing during start-up of the UPS.

    Front View of the UPS

  3. Connect the power cables in the described order. Assemble the cable lugs to the busbars as shown.
    1. Connect the PE cables/equipment grounding conductor (EGC).
    2. Connect the DC cables (DC+, DC-).
    3. Connect the input cables.
    4. Only for dual mains: Connect the bypass cables.
    5. Connect the output cables.

    Cable Lug to Busbar Assembly

    1. Spring washer – provided in kit

    2. Flat washer (not provided)

    CAUTION
    Risk of cable lug disconnection
    • Use the provided spring washers when connecting the cable lugs to the busbars as shown in the illustration.
    • Connect one hole cable lugs and two hole cable lugs to the busbars as shown in the illustration.
    Failure to follow these instructions can result in injury or equipment damage.
  4. Reinstall the transparent plastic protectors (marked (A) on the illustration) and the plastic box (marked (B) on the illustration) in the original position.
    NOTE: On newer UPS models, the box (marked (C) on the illustration) is integrated in the inner door of the UPS instead of being a separate part.

    Front View of the UPS Model with Separate Plastic Box

    Front View of the UPS Model with the Box Integrated in the Inner Door

    CAUTION
    Risk of arc flash and overheating
    The transparent plastic protectors and the plastic box must be reinstalled in the original position after power cabling is completed. Note: On newer UPS models, the box is integrated in the inner door of the UPS instead of being a separate part.
    Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?