Installation Procedure for UPS
![]() |
---|
Hazard of electric shock, explosion, or arc flash
The UPS must be secured against movement. Perform one
of the following once the UPS is in its final position:
Failure to follow these instructions will result in death or serious injury.
|
- Perform one of the following procedures:
- Without seismic anchoring: Position the UPS.
- With seismic anchoring: Install the Seismic Anchoring and Position the UPS.
- Perform one of the following procedures:
- Top cable entry: Prepare the UPS for Top Cable Entry.
- Bottom cable entry: Follow in the installation manual provided with the bottom entry cabinet.
- Only for TNC or HRG earthing system:
- Perform one of the following procedures:
- Connect the Signal Cables.
- Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products.
- Connect the Modbus Cables.
- Only for parallel system: Connect the PBUS Cables.
- Only for external synchronization: Connect the Signal Cables for External Synchronization.
- Option: Install the ERMS Door Switch Kit GVLOPT011 (Option).
- Install the Power Module(s).
- Add Translated Safety Labels to Your Product.
- Final installation.