990-91734-001

Connect the Signal Cables Between the Transformer Cabinets and the UPS in a Single Mains System

  1. Connect the signal cable 0W13741 (transformer thermal sensor) to the cable connection point in the input transformer cabinet and route the signal cable as shown to the UPS and connect.
  2. Connect the signal cable 0W13735 (UIB AUX switch) to the cable connection point in the input transformer cabinet and route the signal cable as shown to the UPS and connect.
  3. Connect the provided signal cable 0W13741, signal cable 0W13697, and signal cable 0W13736 between the output transformer cabinet and the UPS as shown.

    Single Mains System

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?