990-91734A-001

Install the Busbars Between the Transformer Cabinets in a Single Mains System

  1. Install the busbar 880-63679 between the transformer cabinets.

    Front View of the Transformer Cabinets

  2. Install busbar 880-63674, busbar 880-63675, and busbar 880-63676 on the UIB breaker in the input transformer cabinet. Install three busbars 880-63678 in the side of the input transformer cabinet. Install the busbar 880-63729 and busbar 880-63730 between the input transformer cabinet and the output transformer cabinet.

    Front View of the Input Transformer Cabinet, the Output Transformer Cabinet and the UPS

  3. Install busbar 880-63686, busbar 880-63687, and busbars 880-63688 between the UIB breaker and terminals in the right side of the input transformer cabinet. Install busbar 880-63685 on 880-63688 as shown.

    Front View of the Input Transformer Cabinet, the Output Transformer Cabinet and the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?