990-91734-001

Install the Seismic Anchoring (Option)

Use the optional seismic kit GVLOPT002 (for the UPS) and GVLOPT008 (for the transformer cabinets) for this procedure.

  1. Connect the rear anchoring assemblies for the UPS and the transformer cabinets with the interconnection plates.

    Rear View

  2. Mount the rear anchoring assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø16 mm. Minimum requirement is M12 strength grade 8.8 hardware.

    Rear View

  3. Remove the M6 screws and the interconnection plates.

    Rear View

  4. Remove the rear anchoring brackets.

    Rear View

  5. Install the rear anchoring brackets on the UPS and the transformer cabinets with the provided bolts.

    Rear View of the UPS and the Transformer Cabinets

  6. Install the front anchoring brackets on the UPS and the transformer cabinets with the provided bolts.

    Front View of the Transformer Cabinets and the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?