990-91734A-001

Connect the Signal Cables Between the Transformer Cabinets and the UPS in a Dual Mains System

  1. Connect the signal cable 0W13742 (transformer thermal sensor) to the cable connection point in the input transformer cabinet (UIB) and route the signal cable as shown to the UPS and connect.
  2. Connect the signal cable 0W13737 (UIB AUX switch) to the cable connection point in the input transformer cabinet (UIB) and route the signal cable as shown to the UPS and connect.
  3. Install the SSIB breaker indicator light in the input transformer cabinet (SSIB) (the parts are provided in the SSIB kit GVLOPT010):
    1. Install the SSIB breaker indicator light in the bracket in the input transformer cabinet (SSIB).
    2. Connect the signal cable 0W20109 (HSSIB+ and HSSIB-) to the SSIB breaker indicator light (+ and -).
    3. Route the signal cable 0W20109 from the SSIB breaker indicator light as shown to the UPS and connect.
  4. Connect the signal cable 0W13741 (transformer thermal sensor) to the cable connection point in the input transformer cabinet (SSIB) and route the signal cable as shown to the UPS and connect
  5. Connect the signal cable 0W13739 (SSIB AUX switch) to the cable connection point in the input transformer cabinet (SSIB) and route the signal cable as shown to the UPS and connect.
  6. Connect the provided signal cable 0W13697, signal cable 0W13741, and signal cable 0W13736 between the output transformer cabinet and the UPS as shown.

    Dual Mains System

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?