990-91734A-001

Install the Busbars Between the Transformer Cabinets in a Dual Mains System

  1. Install three interconnection busbars TME14246 between the input transformer cabinet (UIB) and the input transformer cabinet (SSIB).

    Front View of the Transformer Cabinets and the UPS

  2. Install two busbars 880-63679 between the transformer cabinets.

    Front View of the Transformer Cabinets

  3. Install two busbars 880-63682, busbar 880-63684, and two busbars 880-63677 on the UIB breaker in the input transformer cabinet (UIB).

    Front View of the Input Transformer Cabinet (UIB)

  4. Install busbar 880-63674, busbar 880-63675, and busbar 880-63676 on the SSIB breaker in the input transformer cabinet (SSIB). Install three busbars 880-63678 in the side of the input transformer cabinet (SSIB). Install the busbar 880-63729 and busbar 880-63730 between the input transformer cabinet (SSIB) and the output transformer cabinet.

    Front View of the Input Transformer Cabinet (SSIB) and the Output Transformer Cabinet and the UPS

  5. Install busbar 880-63686, busbar 880-63687, and busbars 880-63688 between the SSIB breaker and terminals in the right side of the input transformer cabinet (SSIB). Install busbar 880-63685 on 880-63688 as shown.

    Front View of the Input Transformer Cabinet (SSIB) and the Output Transformer Cabinet and the UPS

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?