990-5914B-001

Connect the Power Cables

DANGER
hazard of electric shock, explosion, or arc flash
Perform a total power off of the UPS system before connecting the battery cables to the battery breaker box.
Failure to follow these instructions will result in death or serious injury.
DANGER
Hazard of electric shock, explosion, or arc flash
For TT and TN systems each stand alone cabinet of the system must be individually connected to the protective earthing terminal in the distribution board that supplies the system.
Failure to follow these instructions will result in death or serious injury.
WARNING
Hazard of arc flash
Use the provided M10 bolts and nuts to connect the power cables.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Lockout/Tagout the battery breaker.
  2. Route the PE cables from the UPS cabinet through either the top or bottom of the battery breaker box and connect.

    Cables from the UPS Cabinet Routed through the Top of the 20-80 kW Battery Breaker Box

    Cables from the UPS Cabinet Routed through the Bottom of the 20-80 kW Battery Breaker Box

    Cables from the UPS Cabinet Routed through the Bottom of the 100-200 kW Battery Breaker Box

  3. Route the DC cables from the UPS cabinet through either the top or bottom of the battery breaker box and connect.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Reinstall the inner cover in the top of the battery breaker box before continuing with the installation.
    Failure to follow these instructions will result in death or serious injury.
  4. Route the battery cables from the battery bank through the bottom of the battery breaker box and connect.
    DANGER
    hazard of electric shock, explosion, or arc flash
    • Reinstall the inner cover in the bottom of the battery breaker box before continuing with the installation.
    • Ensure correct polarity.
    Failure to follow these instructions will result in death or serious injury.
  5. Attach the cables to the cables reliefs in the left side, the top, and the bottom of the battery breaker box.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.