990-5914B-001

Connect the Signal Cables

  1. Loosen the screws of the protection covers and lift the protection covers up and out of the battery breaker box.

    Front View of the 20–80 kW Battery Breaker Box

    Front View of the 100–200 kW Battery Breaker Box

  2. Route the signal cables through the bottom of the battery breaker box. For the 20–80 kW you can also route the signal cables through the top of the battery breaker box.
  3. Remove the cover on the battery breaker.

    Front View of the Battery Breaker Box

  4. Connect the signal cables:
    1. Connect the signal cables to the AUX switch.
    2. Connect the signal cables to the undervoltage trip coil.
    3. Fasten the signal cables with cable ties (provided) to the cable relief.

    Front View of the Battery Breaker Box

  5. Reinstall the cover on the battery breaker.
  6. Route the signal cables separately from the power cables.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.