990-5913E-001

Connect the Signal Cables to the Galaxy VS UPS

NOTE: Route the signal cables separately from the power cables to ensure sufficient isolation.
NOTE: Use double isolated signal cables. The signal cables must have a minimum rating of 600 V.
  1. Install the temperature sensor provided with the UPS in the top of the classic battery cabinet.
    WARNING
    Hazard of fire
    Position the temperature sensor as described to ensure correct temperature measurements.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    GVSCBC7C, GVSCBC7D, GVSCBC7E

    GVSCBC10A2, GVSCBC10B2

  2. Route the battery temperature sensor cables through the bottom of the classic battery cabinet to the UPS and connect as shown.
    NOTE: One temperature sensor is provided with the UPS. Contact Schneider Electric if you want to buy an additional temperature sensor (0J-0M-1160).
    NOTE: The battery temperature sensor cables are considered Class 2 and SELV. Class 2 and SELV circuits must be double isolated from the primary circuitry.
  3. Remove the cover on the battery breaker.
  4. Connect the signal cables to the battery breaker:
    1. Connect the signal cables to the AUX switch.
    2. Connect the signal cables to the undervoltage trip coil.
    3. Route the signal cables out through the lower opening of the battery breaker.
  5. Route the signal cables from behind the battery breaker and out through the bottom of the classic battery cabinet.

    Rear View of the Battery Breaker

  6. Reinstall the cover on the battery breaker.
  7. Connect the signal cables in the UPS as shown.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.