990-5913E-001

Final Installation

  1. Install the provided kick plates on the front, rear, and sides of the classic battery cabinet.
    NOTE: Only remove the kick plates when following the procedure for decommissioning or moving the classic battery cabinet. See Decommission or Move the Classic Battery Cabinet to a New Location for details.
  2. Close the door(s). On GVSCBC10A2 and GVSCBC10B2, install two screws to close the left door.

    GVSCBC10A2, GVSCBC10B2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.