990-91260F-001

Connect the Signal Cables from Switchgear and Third-Party Auxiliary Products

NOTE: Route the signal cables separately from the power cables and route the Class 2/SELV cables separately from the non-Class 2/non-SELV cables.

Maximum Disconnect Device Configuration in Single System with Third-Party Switchgear

NOTE: IMB* cannot be used in a system with an external MBB and IMB* must be padlocked in the open position.
  1. Connect signal cables from the disconnect device indicator lights in your switchgear to board 640-4864 terminal J6618 in the top of the UPS. If an external supply is used, remove jumper from J6618 pin 8 and 9.
    NOTE: The disconnect device indicator light circuit is considered Class 2/SELV. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the disconnect device indicator light terminals unless it can be confirmed that the circuit is Class 2/SELV.
  2. Connect signal cables from AUX switches in your switchgear to board 640-4843 in the top of the UPS.
    Terminal number Function Connection
    J6601 UOB_RED (redundant AUX switch in unit output disconnect device) Connect to redundant AUX switch in unit output disconnect device UOB.
    J6602 SIB (system isolation disconnect device) Connect to normally open (NO) AUX switch in system isolation disconnect device SIB for parallel system. SIB must contain an AUX switch for each connected UPS.
    J6609 UOB (unit output disconnect device) Connect to normally open (NO) AUX switch in unit output disconnect device UOB.
    SSIB (static switch input disconnect device) Connect to normally open (NO) AUX switch in static switch input disconnect device SSIB. SSIB must contain an AUX switch for each connected UPS.
    J6614 UIB (unit input disconnect device) Connect to normally open (NO) AUX switch in unit input disconnect device UIB. UIB must contain an AUX switch for each connected UPS.
    MBB (maintenance bypass disconnect device) Connect to normally closed (NC) AUX switch in maintenance bypass disconnect device MBB. MBB must contain an AUX switch for each connected UPS.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?