990-91260F-001

Final Installation

DANGER
Hazard of electric shock, explosion, or arc flash
Batteries can present a risk of electric shock and high short-circuit current. The following precautions must be observed when working on batteries
  • Remove watches, rings, or other metal objects.
  • Use tools with insulated handles.
  • Wear protective glasses, gloves and boots.
  • Do not lay tools or metal parts on top of batteries.
  • Disconnect the charging source prior to connecting or disconnecting battery terminals.
  • Determine if the battery is inadvertently grounded. If inadvertently grounded, remove source from ground. Contact with any part of a grounded battery can result in electric shock. The likelihood of such shock can be reduced if such grounds are removed during installation and maintenance (applicable to equipment and remote battery supplies not having a grounded supply circuit).
Failure to follow these instructions will result in death or serious injury.
WARNING
risk of equipment damage
Wait until the system is ready to be powered up before installing batteries in the system. The time duration from battery installation until the UPS system is powered up must not exceed 72 hours or 3 days.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Reinstall the top cover:
    1. Tilt the top cover and slide it onto the UPS from the rear. Taps in the rear of the top cover must connect to the slots in the rear of the UPS.
    2. Push the top cover down in the front.

      Rear View of the UPS

    3. Reinstall the screws.
  2. Remove the rear transportation bracket from the UPS.
  3. Only for seismic anchoring:
    1. Install rear anchoring bracket on the UPS with the provided M8 bolts.

      Rear View of the UPS

    2. Push the UPS into position so the rear anchoring bracket connects to the rear anchor.

    Rear View of the UPS

  4. Lower the front and rear leveling feet on the UPS with a wrench until they connect with the floor. Use a bubble-leveler to check that the UPS is level.
    NOTICE
    Risk of Equipment damage
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.
  5. Only for non-seismic anchoring: Mount the front transportation bracket to the floor. The UPS can be top-heavy and tip over if not bolted to the floor. Use appropriate hardware for the floor type – the hole diameter in the front transportation bracket is ø9 mm
  6. Only for seismic anchoring:
    1. Remove the front transportation bracket from the UPS.
    2. Install the seismic front anchoring bracket on the UPS.
    3. Mount the seismic front anchoring bracket on the UPS to the floor. Use appropriate hardware for the floor type – the hole diameter in the seismic front anchoring bracket is ø18 mm.
  7. Set the battery disconnect device BB to the open (OFF) position.
  8. Push extra battery modules (if any) into the slot. Fill the shelves from the bottom and upwards.
  9. Turn down the battery module handle on the extra battery modules and fasten the handle to the shelf with the provided screw.
  10. Connect the battery terminals to the front of the battery modules.
  11. Reinstall all plates and covers removed in Prepare for Installation.
  12. Reinstall the front panel on the UPS:
    1. Insert the two taps in the bottom of the front panel in the UPS at a tilted angle.
    2. Reconnect the front panel strap to the UPS.
    3. Close the front panel and lock with the two locking knobs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.