990-5783J-001

Final Mechanical Assembly

Final Mechanical Assembly of the I/O Cabinet

DANGER
hazard of electric shock, explosion, or arc flash
All panels and covers must be properly reinstalled prior to energizing the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Lift up the Class 2/SELV cables.

    Front View of the I/O Cabinet

  2. Reinstall the indicated box over the non-Class 2/non-SELV cables.
  3. Reinstall the indicated box over Class 2/SELV cables.

    Front View of the I/O Cabinet

  4. Reinstall the plate over the cable channel for non-Class 2/non-SELV cables.
  5. Reinstall the two plates in the left side.

    Front View of the I/O Cabinet

  6. Reinstall the plate in the right side.

    Front View of the I/O Cabinet

  7. Reinstall the six plates in the left and right sides of the I/O cabinet.

    Front View of the I/O Cabinet

  8. Reinstall the two metal plates.

    Front View of the I/O Cabinet

  9. Close the front doors.

Final Mechanical Assembly of the Power Cabinets

DANGER
hazard of electric shock, explosion, or arc flash
All panels and covers must be properly reinstalled prior to energizing the UPS.
Failure to follow these instructions will result in death or serious injury.
  1. Reinstall the three plates in the given order (a-c) on each power cabinet.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?