Torque Specifications
![]() |
---|
Hazard of electric shock
All electrical connections must be torqued according to
this table.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Bolt size |
Torque |
---|---|
M6 |
5 Nm (3.69 lb-ft) |
M8 |
17.5 Nm (12.91 lb-ft) |
M10 |
30 Nm (22 lb-ft) |
M12 |
50 Nm (36.87 lb-ft) |