990-5783J-001

External Communication

The following interfaces are supported:

  1. Two smart slots for optional network management cards (AP9630, AP9631, AP9635CH).

    NOTE: If the input dry contact AP9810 is connected to AP9631 or AP9635CH, the total length of cables for connected equipment must not exceed 30 m (98 ft). Use the plate for shielding.
  2. Modbus and modbus dip switch settings.

  3. Network/ethernet.

Front View of the I/O Cabinet

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?