Mount the Rear Anchoring Brackets
![]() |
---|
hazard of tilting
All rear and front anchoring brackets must be installed.
Failure to follow these instructions will result in death or serious injury.
|
![]() |
---|
hazard of electric shock, explosion, or arc flash
Leave the UPS system covered while making anchoring holes
to prevent dust or other conductive particles from entering the system.
Failure to follow these instructions will result in death or serious injury.
|
- Use the rear anchoring bracket that was attached to the rear of the I/O cabinet pallet. Fasten the two plates from the installation kit 0H-9101 to the rear anchoring bracket of the I/O cabinet with M8 bolts. Note the direction of the plates.
- Place the rear anchoring brackets for the I/O cabinet and the power cabinets in the final installation area.
- Interconnect the rear anchoring brackets using the provided screws and bolts.
- Mark the hole locations.
- Drill anchoring holes according to the national and local requirements.
- Mount the rear anchoring brackets to the floor. Bolts are not supplied.
- Use a bubble-leveler to ensure that the rear anchoring brackets are level. Use the provided leveling shims if necessary.