Storage
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Always repack cabinets and modules to their original delivered
packing condition. Moisture inside cabinets or modules can create
hazardous short circuits.
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
Damaged Batteries
Never store batteries more than 6 months. If the batteries
are de-energized for a long period of time, the batteries must be
charged for 24 hours at least once every month.
Failure to follow these instructions can result in equipment damage.
|
If the system, modules or batteries needs to be stored a short time after delivery but before installation, the system should be stored in the transportation crate with the sealed inner packing intact.
If the system, modules or batteries needs to be stored for a longer period of time please refer to the information in the sections:
Recommended Storage Environments
- Storage temperature:
-
Battery: See recommendations from the original equipment manufacturer (OEM).
-
System and modules : -10 °C to +55 °C (+14 °F to +131 °F)*
-
-
Relative humidity: 0–95% Non-condensing
DANGER