0000670338_02_en

Unpack the System from the Crate/Frame

CAUTION
risk of crushing and Sharp edges
Always use protective gloves when unpacking the system.
Failure to follow these instructions can result in injury or equipment damage.

Use the right tool depending on the construction of the crate/frame:

  • For screws use a screwdriver.

  • For metal clamps use a flat screwdriver.

NOTE: For solid crates it is not necessary to remove the skids.

  1. Remove the top with the correct tool.

  2. Remove the side walls with the correct tool one after another until all side walls are removed.

Now the system is on the pallet with the inner packing protection.

NOTE: Always dispose of any waste in accordance with local regulations and rules.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?