0000670338_02_en

Unpacking

WARNING
Short Circuit
Never install a system with moisture inside the cabinet, it can create hazardous short circuits. To protect the system from moisture:
  • Only unpack the system just before installation.
  • Always unpack the system in a clean and dry environment.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Unpack the system in a clean and dry (humidity < 60%) storage area.

If the system is not completely dry, for example if there is any moisture or condensed water, let the system stand with the cabinet doors open in a dry and warm area for at least 24 h.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?