0000670338_02_en

Transport the Crate Before Unpacking

WARNING
heavy object
When transporting the crate always pay attention to the placement of the center of gravity markings.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: The gross weight of the crate is printed on the crate.

When transporting the crate make sure to check:

  • That the transport equipment can carry the weight and size of the crate in a safe way.

  • Observe the position of the center of gravity on the crate, make sure it is correctly placed.

  • Make sure that the crate is positioned correctly on the forks.

  • Make sure that the floor can support the weight of the system during transport.

Before unpacking remove the delivery note that is attached in an envelope on the side of the crate. Keep the delivery note to check that the description and quantity of all the items of the packing list is correct. If any discrepancies are found this must be reported to Gutor Service Center as soon as possible.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?