0000670338_02_en

Packing Process Information

CAUTION
hazardous chemicals
Some packaging options use volatile corrosion inhibitor (VCI). When in contact with VCI:
  • Make sure the area is well ventilated.
  • Always use protective gloves when handling VCI materials.
  • Do not eat, drink or smoke nearby.
  • Always wash your hands and exposed skin after handling VCI materials.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
Loss of package protection
To ensure that the packing material protects the system:
  • Open the protective packing just before installation.
  • If opened for inspection, re-seal the packing material quickly and to the initial condition.
  • Make sure the packing material does not get any scratches or cuts.
Failure to follow these instructions can result in equipment damage.

The inner and outer packing options depends on customer requests, country of origin and type of freight (land, sea, air).

Inner packing options:

  • Plastic wrap

  • VCI plastic cover

  • Vacuum sealed aluminium foil

NOTE: There are multiple variations of the inner packing options. There can be different types on extra protections like foam, rubber pads, paper, additional layers or combinations of options.

Outer packing options:

  • Solid wood frame

  • Plywood crate

  • Solid wood crate

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?