0000670338_02_en

Symbols for Markings on the Crate

WARNING
heavy object
When transporting the crate always pay attention to the placement of the center of gravity markings.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The transportation crate is marked with the following standardized symbols to indicate how to handle, store and transport the transportation crate. For more information about how to transport the crate see the chapter Transport the Crate Before Unpacking.

Symbol

Description

This side up: The crate must be stored, moved and transported so that the arrows are always pointing up.

Fragile. Handle with care: The crate contains fragile goods. Handle the crate with care to not damage the goods.

Center of gravity: Indicates the center of gravity of the crate. Always be aware of the center of gravity when lifting and moving the crate.

Keep away from rain: Do not expose the crate to rain or wet conditions.

Do not stack: It is not allowed to place anything on top of the crate or frame.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?