0000670338_02_en

Unpack the System

NOTE
Parts delivered in separate packages
Be careful when unpacking the system that none of the packages or bags with parts for installation are thrown away.

When any crate or frame have been removed continue to unpack the system by:

  1. If applicable, remove the vacuum sealed aluminium foil or VCI plastic.

  2. If applicable, remove any protective plastic, paper, felt and/or foam.

  3. If applicable, remove any desiccant bags.

  4. If applicable, remove any VCI-foam strips placed inside the system.

  5. The system is delivered on a customized pallet.

  6. Loose parts are delivered under the rain roof on top of the system and/or inside the cabinet.

  7. The modules and any batteries will be delivered in a separate crate/pallet (typically either EUR-pallet or EUR-6-pallet).

  8. Examine the inside of the system for any transportation damage. If any damage is found, immediately contact both the shipping agency and Gutor Service Center.

  9. The system is now ready to be moved to the installation site. For more information see the Installation Manual.

NOTE: Always dispose of any waste in accordance with local regulations and rules.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?