VIGED310022EN-06

Cumplimiento de normas aplicables en China

Este producto cumple las siguientes normas aplicables en China:

BS/EN/IEC 61557-8 Electrical safety in low voltage distribution systems up to 1 000 V a.c. and 1 500 V d.c. - Equipment for testing, measuring or monitoring of protective measures - Part 8: Insulation monitoring devices for IT systems

Comentarios
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.