JYT1078000

Reference Publications

Schneider Electric publications are available through a local Schneider Electric representative. These publications include device replacement procedures and listings of spare parts to make ordering and servicing of replacement parts quick and convenient. Any maintenance procedure or device not listed, such as an
I-Line interior, is not customer serviceable.

Contact a local Schneider Electric representative for information at 1-888-778-2733. Or, refer to the Technical Library at http://www.se.us/ to obtain the appropriate publications.

For information about obtaining NEMA documents, write to:

National Electrical Manufacturers Association (NEMA)
Attention: Customer Service
1300 North 17th Street
Suite 1847
Rosslyn, VA 22209

Other Reference Publications Publication Number
General Instructions for Proper Installation, Operation, and Maintenance of Switchboards Rated 600 V or Less NEMA Publication PB2.1
Application Guide for Ground Fault Protective Devices for Equipment NEMA Publication PB2.2
Circuit Breakers NEMA Publication AB-4
Enclosed and Miscellaneous Distribution Switches NEMA Publication KS-1
Electrical Equipment Maintenance NFPA 70B-1999

Spare Parts Support

For spare parts ordering support contact the Schneider Electric Customer Care Center at 888-778-2733.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.