JYT1078000

Receiving, Handling, and Storing

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
If signs of moisture contamination are present, do not follow the instructions in this section; proceed to Moisture Contamination Avoidance and Mitigation.
Failure to follow these instructions will result in death or serious injury.

Receiving

Upon receipt, check the packing list against the equipment received to ensure the order and shipment are complete. Also, upon receipt, immediately inspect switchboard sections for any damage that occurred in transit. If damage is found or suspected, file a claim with the carrier immediately and notify the nearest Schneider Electric representative.

Handling

NOTICE
hazard of structural Damage
  • Do not lay the equipment on its front or sides.
  • Lay equipment on its back only when special handling is required.
  • Do not ship the equipment in a horizontal position.
Failure to follow these instructions can result in equipment damage.

Ensure that proper equipment, such as an overhead crane, is available at the installation site to handle the switchboard. This equipment helps avoid injury to personnel and damage to the switchboard.

The shipping weight of each shipping section is marked on the packing list. Verify the lifting capacity of the equipment being used to handle the switchboard in accordance with the shipping weight of each shipping section. Keep the switchboard upright during handling.

Schneider Electric recommends using an overhead crane, lifting straps, and cables or chains to handle the switchboard. This method and alternative handling methods are discussed in this section.

Handling with Lifting Straps

Schneider Electric provides lifting eyes as standard equipment for FlexSeT switchboards. Instruction labels on each shipping section include drawings and written instructions outlining the proper use of the lifting straps (see Lifting with an Overhead Crane, Lifting Straps, and Cables or Chains). Use rigid spreaders or a spanner bar to provide vertical lift on the lifting straps. This helps avoid damage to the frame or finish.

Lifting with an Overhead Crane, Lifting Straps, and Cables or Chains

Handling Instruction Label-Switchboards with Lifting Straps

Follow these instructions to handle the switchboard:

  1. When attaching lifting straps to the switchboard, assemble the hardware in the order shown in Hardware Assembly Order. In enclosures with rear and front vertical corner channels with knockouts, remove the top-most 0.5 in. (13 mm) diameter knockout and assemble the hardware in the order shown in Hardware Assembly Order in Enclosures With Knockouts in Vertical Corner Channels.
    NOTE: In some cases, the lifting straps may come pre-assembled in the FlexSeT switchboard from factory, if this is the case, skip step 1.

    Hardware Assembly Order

    Hardware Assembly Order in Enclosures With Knockouts in Vertical Corner Channels

  2. Use load-rated cables or chains with safety hooks* or shackles. Do not pass cables or chains through holes in lifting straps.
  3. Use a load-rated spreader beam to help prevent structure damage. Rig so that the minimum angle between the lifting cables or chains and equipment top is 45°.
  4. Once the lifting straps have been used, remove them from the enclosure by removing the nut and the rest of the hardware shown in Hardware Assembly Order. In the case of enclosures with rear and front vertical corner channels that include knockouts, once the lifting straps have been removed, close the knockouts openings in the rear and front vertical channels using the provided plastic caps, as shown in Hardware Assembly Order in Enclosures With Knockouts in Vertical Corner Channels.

Handling without Lifting Straps

Lifting eyes are not furnished on skid mounted or outdoor subassembly. Use rollers, slings, or other means to handle the shipping sections. The handling label (see Handling Instruction Label-Switchboards without Lifting Straps) is affixed to each of these sections.

Handling Instruction Label-Switchboards without Lifting Straps

WARNING
Hazard of TOP HEAVY LOAD-TIPPING
  • Stabilize the shipping section to reduce the possibility of tipping.
  • Consult with a certified rigging and lifting expert for any situation not covered in these instructions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

When elevating a shipping section not equipped with lifting eyes, use an overhead crane equipped with either of the following:

  • A chain coupled to a sling rigging. Wrap the sling completely around the switchboard and shipping stringers.
  • A wire cable with safety hooks and shackles.

A forklift is an alternative method of handling the switchboard. Before using a forklift:

  • Read the fork access labels on the switchboard sections (see Handling with a Forklift).
  • Check the fork lengths to ensure the forks extend under the entire switchboard.
  • Carefully balance the load.
  • Use a strap when handling or moving a switchboard with a forklift.

Handling with a Forklift

Storage

When storing the switchboard before installation, cover the top and openings 
of the equipment during the construction period to help protect the switchboard from dust and debris.

If a switchboard is not installed and energized immediately, store it in a clean, dry space with a consistent temperature to help prevent condensation. Store the switchboard indoors, if possible. Preferably, store it in a heated building with adequate air circulation and protect it from dirt, fumes, water, and physical damage. Storing the switchboard outdoors can cause harmful condensation inside the switchboard.

NOTE: Install portable electric heaters of approximately 250 W per vertical section in both indoor-type and rainproof-type switchboard enclosures for adequate protection during storage.

Before energizing the space heaters, remove all loose packing or flammable materials inside the switchboard. Outdoor switchboards are not weather-resistant until completely and properly installed; treat them the same as indoor switchboards until after installation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.