JYT1078000

Adverse Circumstances

This section includes, but is not limited to, all electrical components of the switchboard.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462 or local equivalent.
  • This equipment must be installed and serviced only by qualified personnel.
  • Perform such work only after reading and understanding all of the instructions contained in this bulletin.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Before performing visual inspections, tests, or maintenance on this equipment, disconnect all sources of electric power. Assume all circuits are live until they are de-energized, tested, and tagged. Pay particular attention to the design of the power system. Consider all sources of power, including the possibility of backfeeding.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Handle this equipment carefully and install, operate, and maintain it correctly for it to function properly.
  • Carefully inspect the work area and remove any tools and objects left inside the equipment.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • All instructions in this manual assume that the customer has taken these measures.
Failure to follow these instructions will result in death or serious injury.
NOTE: Before attempting to re-energize the switchboard following adverse circumstances, contact Schneider Electric Services at 1-888-778-2733 (US) for special instructions.

Inspection Following a Short Circuit

If a short circuit occurs, make a thorough inspection of the entire system, and verify that no damage to conductors or insulation has occurred. High mechanical and thermal stresses developed by short-circuit currents can damage conductors and insulation. Check the overcurrent-protection device that interrupted the short-circuit current for possible arcing damage.

Do not open sealed devices, such as molded case circuit breakers. Replace these devices if they are damaged. Before energizing the switchboard, all unused circuit breaker mounting spaces must be filled. For more information about these devices, refer to the appropriate instruction manual listed in Reference Publications.

Clean-up Following a Short Circuit

The insulating properties of some organic insulating materials can deteriorate during an electrical arc. If so:

  1. Remove any soot or debris.
  2. Replace carbon-tracked insulation.

Water-Soaked Switchboards

Do not clean or repair a switchboard that has been exposed to large volumes of water or submerged at any time. Current-carrying parts, insulation systems, and electrical components may be damaged beyond repair. Do not energize the switchboard. Contact Schneider Electric Services at 1-888-778-2733 (US).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.