DOCA0182EN-06

Firmware Update Policy

If the latest features of a firmware update are not required, it is not mandatory to update the firmware of a device. However, potential cybersecurity vulnerabilities are regularly addressed and update is recommended.

Use this release note to determine whether an update to the latest version of the Link150 firmware is interesting or relevant for your application.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?