DOCA0182EN-06

Firmware Version 005.001.024

Security Updates

  • Removed the support for TLS 1.0 and TLS 1.1.

  • Disabled the TCP option Timestamp.

  • Included the Treck TCP stack patch for IPv6 vulnerabilities.

New Features

Added the user certificate management feature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?