DOCA0182EN-06

Firmware Version 005.001.022

New Features

  • Added the configurable Modbus port numbers for remote device connections in Modbus Slave mode.

  • Added a feature to disable the Ethernet port not in use.

  • Added the security updates in support of SNMP default configurations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?