DOCA0182EN-06

Firmware Upgrade via Firmware Upgrade Tool

The Link150 Firmware Upgrade Tool provides the software solution to update the Link150 gateway to the latest firmware version irrespective of the initial version.

The tool is included inside the Link150 firmware update (v5.3.7) package, available as a ZIP file. Once extracted, the Mass Upgrade tool can be used to initiate the firmware upgrade.

You can download the latest version of this tool from the Schneider Electric website: https://www.se.com/in/en/download/document/FW_v5.3.7/. For the latest version number of the tool, refer DOCA0304EN – Link 150 Ethernet Gateway Firmware Upgrade Tool Release Notes.

The firmware update procedure is detailed in DOCA0223EN – Link150 Ethernet Gateway Firmware Upgrade Tool – User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?