Firmware Version 005.001.015
Security Updates
-
Security updates in support of:
-
Self-signed certificate
-
Link150 gateway in HTTPS Enabled mode by default
-
RBAC-User Account Management supported with Admin and Guest pre-defined roles
-
-
Removed the FTP feature for better security
New Features
Added the following features:
-
New user interface layout in the webpages
-
RSTP feature
-
Firmware update supported through webpage for version 005.001.015
-
Firmware version 005.001.015 is not backward compatible with existing User Account Management. By updating to firmware version 005.001.015, user will lose all the user account settings.
-
Connection of Modbus TCP/IP cannot be configured from firmware version 005.001.015, and supports up to 32 address.
-
Link150 gateway with firmware version 005.001.015 cannot be downgraded to older version of firmware (up to version 005.000.029).