DOCA0182EN-06

Link150 Ethernet Gateway

Link150 Ethernet gateway is a communication device that provides connectivity between Ethernet (Modbus TCP/IP) and Modbus serial line devices.

It allows:

  • Modbus TCP/IP clients to access information from serial slave devices

  • Serial master devices to access information from slave devices distributed across an Ethernet network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?