6055-40 Rev. 02

Introduction

This instruction bulletin contains instructions for receiving, handling, storage, installation, operation, and maintenance for the Masterclad 27 kV drawout, metal-clad switchgear manufactured by Schneider Electric. This equipment is designed for use with the 27 kV drawout circuit breaker, which uses vacuum technology.

For information on the 27 kV circuit breakers, refer to instruction bulletin 6055-41.

The switchgear assembly consists of individually-grounded steel compartments. Each compartment has doors, barriers, and removable access panels to isolate the separate working functions. All the circuit breakers, relays, meters, and other components are factory-assembled, wired, and tested as an assembly. The user normally makes only the external control, ground, and power connections at the terminations, and reconnects the wiring and busbars at the shipping breaks.

Each assembly is custom designed to specifications. Standard enclosures and bus configurations are arranged according to customer specifications.

Complete customer drawings are furnished for each Masterclad switchgear assembly. The drawings include floor plans, front elevations, one-line diagrams, control schematics, and wiring diagrams.

27 kV Masterclad Indoor Switchgear with Circuit Breaker

Product Overview

This section contains a basic overview of the workings of the Type VR, 27 kV switchgear and the identification of certain components.

A Masterclad switchgear line-up assembly consists of individual switchgear bays that are bolted together. The number of bays in an assembly depends on customer specifications.

Each switchgear bay is a separate rigid, self-contained, bolted structure made of heavy gauge steel. A switchgear bay consists of:

  • Front section with secondary control devices

  • Circuit breaker compartment

  • Main bus compartment

  • Cable compartment

  • Drawout voltage transformer (optional)

  • Control power transformer (optional)

  • Fuse drawout section (optional)

  • Surge arrestor (optional)

Front Section with Secondary Control Devices

The front section includes the front hinged doors with instruments, relays, control switches, terminal blocks, fuse blocks, and other required secondary control devices. It also houses the wiring space for inter-unit connection and customer control wiring connection.

Circuit Breaker Compartment

The circuit breaker compartment contains separate, but coordinated, features.

Circuit Breaker Compartment

Circuit Breaker Positioning Rails

Positioning rails, mounted on the side walls of the circuit breaker compartment, capture and align the rollers on the circuit breaker to guide the circuit breaker into the circuit breaker compartment.

The racking mechanism is located on the circuit breaker compartment floor. It is operated by a removable racking handle inserted into the front of the circuit breaker compartment so that it can be racked with the door closed. The circuit breaker engages in a gear-driven racking arm. As the arm rotates, it moves the circuit breaker into or out of the TEST/DISCONNECT or the CONNECTED position.

Secondary Disconnect Receptacle

The secondary disconnect receptacle is located on the lower right floor of the compartment. The molded insulating receptacle contains 24 contacts and two tapered guide pins. Control power can be connected in the test position by rotating the secondary disconnect handle and pulling it forward.

Racking Position Indicator

The racking position indicator, located beside the racking port, indicates if the circuit breaker is in the TEST/DISCONNECT, TRANSPORT, or CONNECTED position. When the door is open, two arrows that line up with the front cover are visible on the left rail and indicate the position of the circuit breaker.

Primary Contacts

The primary contacts are housed in primary bushing assemblies that are covered at the open end by the shutter when the circuit breaker is in the TEST/DISCONNECT position.

Current Transformer

Window-type, 600 V, rated single- or multi-ratio current transformers are located around either the line or load primary 27 kV insulated bushings. A maximum of four current transformers, depending on accuracy, can be mounted per phase-two on the line, two on the load.

Ground Contact Bar

A ground bar, located on the bottom of the circuit breaker compartment, is directly connected to the main ground bus. Sliding contact fingers, located on the underside of the circuit breaker, engage before the circuit breaker reaches the TEST position and remain continuously grounded.

Mechanism Operated Contacts (Optional)

Mechanism operated contacts (MOCs) are compartment-mounted auxiliary contacts that are operated by the circuit breaker mechanism (see Mechanism Operated Contacts (MOCs)). Like circuit breaker mounted auxiliary contacts, they indicate whether the circuit breaker is in the OPEN or CLOSED position. They operate in the CONNECTED and/or TEST/DISCONNECTED positions. Refer to the customer order drawings shipped with your equipment.

NOTE: The NORMALLY-OPEN “A” contacts and the NORMALLY-CLOSED “B” contacts furnished are not convertible.

The MOC unit is mounted on the left side of the circuit breaker compartment. It is operated by a mechanism that is driven vertically by a roller on the left side of the circuit breaker.

Mechanism Operated Contacts (MOCs)

Truck Operated Contacts (Optional)

The truck operated contacts (TOCs) (see Truck Operated Contacts (TOCs)) indicate whether the circuit breaker is in the CONNECTED or TEST/DISCONNECT position in the circuit breaker compartment.

Truck Operated Contacts (TOCs)

The TOC unit does not distinguish between the circuit breaker being in the TEST/DISCONNECT position or withdrawn completely from the compartment.

The TOC unit is mounted on the right side of the horizontal steel barrier in the top of the circuit breaker compartment. It is operated by a spring-loaded lever. This lever is activated, just before the circuit breaker reaches the CONNECTED position, by a pin on the upper right side circuit breaker frame.

Interlocks

NOTICE
interlock damage
  • Do not test interlocks by hand. Test interlocks by moving the circuit breaker over the compartment-mounted operating cams.
  • Do not operate interlocks in an incorrect sequence.
Failure to follow these instructions can result in equipment damage.

Circuit Breaker Compartment Interlocks

The circuit breaker compartment contains the following interlocks:

  • A racking block bar (see Circuit Breaker Compartment) welded to the racking shaft hits an interlock pin on the circuit breaker when it is closed. This interlock mechanism stops a closed circuit breaker from being racked into or out of the circuit breaker compartment.

  • The racking arm actuates an interlock located underneath the circuit breaker. This interlock mechanism is designed to stop a circuit breaker from being closed when it is between the TEST/DISCONNECTED and CONNECTED positions.

  • A racking roller position lockout lever (see Circuit Breaker Compartment) located on the racking gear box stops the circuit breaker from being inserted into the circuit breaker compartment when the racking roller is not in the TEST/DISCONNECT position.

  • A racking block lever (see Circuit Breaker Compartment) does not allow racking mechanism operation when the circuit breaker is not in the circuit breaker compartment. The shutter cannot be opened unless the circuit breaker is in the circuit breaker compartment.

  • A spring discharge cam (see Circuit Breaker Compartment) discharges the closing springs when the circuit breaker is inserted or withdrawn from the circuit breaker compartment.

  • A racking mechanism lockout provision (see Circuit Breaker Compartment) is furnished in each compartment for locking circuit breakers, VT drawout units, or CPT fuse drawouts out of the CONNECTED position.

    The racking mechanism lockout provision is in the center of the compartment floor and has padlock provisions as standard. It can be equipped with a key interlock when specified by the customer.

    The racking mechanism lockout helps prevent the racking of circuit breakers, VTs, or CPTs when they are in the disconnected position. Circuit breakers, VTs, or CPTs can be stored in the disconnected position with the racking mechanism locked.

Compartment Rating Interlock

The compartment rating interlocks (see Circuit Breaker Compartment) block insertion of circuit breakers with incorrect current, voltage, or interrupting ratings into the compartment. The stationary interference brackets are mounted on the floor of the compartment and the mating part of the interlock system is mounted on the underside of each circuit breaker.

Ground and Test / Removable Shorting (RS) Device Interlock

Each circuit breaker compartment may have permissive interlocks (see Circuit Breaker Compartment) that helps block the insertion of a ground and test or a RS device not intended for use in that circuit breaker compartment. The permissive interlocks are beside the compartment rating interlock on the circuit breaker compartment floor. Refer to the specific Schneider Electric ground and test and RS device instruction bulletins.

Voltage Transformer and Fuse Drawout Units

The voltage transformer (VT) and fuse drawout units are self-contained drawers. As the drawout units are racked into the compartments, the drawers roll on two positioning rails mounted on the sides of the compartment. The rails capture and align rollers on drawout units.

Floating, drawer-mounted, self-aligning contacts engage the stationary primary contacts as the drawer is racked into the connected position.

A ground contact bar, located on the left guide rail, is directly connected to the main ground bus.

A sliding contact finger, located on the left side of the drawout units, engages the ground bar when the drawout unit is in the DISCONNECTED position and remains continuously grounded.

A static discharge ground contact, mounted in the top of the compartment, grounds the primary fuse contact tabs during withdrawal from the CONNECTED position to the DISCONNECTED position.

Control power transformers (CPTs) are always stationary mounted. Depending on the size of the transformer, they can be mounted remotely or within the switchgear.

Drawout Voltage Transformers

Drawout voltage transformers supply voltage indication for metering and relaying purposes. Primary current-limiting fuses are mounted on each voltage transformer.

When drawout voltage transformers are in the CONNECTED position, the secondary contacts, mounted on the bottom rear of the drawer, engage fixed compartment floor-mounted secondary contacts.

Secondary fuses for the voltage transformers are in the front control compartment. Refer to the customer order drawings shipped with the equipment.

Drawout Voltage Transformer

Fuse Drawout Unit for the Stationary Control Power Transformers

Drawout fuses are provided for stationary control power transformers. Fixed mounted CPTs are supplied when AC control power is required. The primary current-limiting fuses are mounted in the drawer and withdrawn as an assembly.

Drawout Primary Fuses for Stationary Control Power Transformer

The fuse drawout truck is interlocked with the CPT secondary-main circuit breaker by a key interlock system. The CPT secondary-main circuit breaker and key interlocks are mounted below the primary fuse drawout unit. Two keys are shipped inserted in the interlock barrels. See CPT Primary Fuse Drawout Unit Interlocks for instructions for operating the key interlocks.

Key Interlocks for Drawout Primary Fuses and Secondary Circuit Breaker

Main Bus Compartment

The main bus compartment is in the center of the switchgear. It is isolated from other compartments by the main bus compartment cover, which consists of removable metal access plates. The main bus compartment is accessible from the back through the cable compartment and from the front through the circuit breaker compartment. The main bus is available in copper only.

Bus Compartment

Each busbar has epoxy insulation rated for 221°F (105°C) operation. Glass polyester barriers with epoxy insert pass-throughs are used to separate the bus compartments between adjacent circuit breaker compartments. Bus boots insulate the connection in the main bus compartment, overlapping the epoxy insulation on the busbars. The busbar insulation and boots form an integral insulating system for the equipment to meet its dielectric ratings. The busbar insulation must not be damaged or modified. Boots must be in place before operating the equipment.

Cable Compartment

Each circuit breaker in a vertical section has a separate cable compartment, accessible by removing a steel cover on the back. Insulated load connectors are provided for terminating cables. As standard, the load connectors are punched for terminating two cables per phase with a NEMA two-hole pattern.

A ground bus in the cable compartment has lugs on each end for the assembly ground. This ground bus is connected to each circuit breaker compartment ground contact bar and to the individual ground bars in each cable compartment. All instrument transformer, metering, and relaying grounds are also connected to this common ground system.

Conduit must enter the cable compartments, in the areas shown on the customer drawings (see Main Bus Connections, Side View), from either the top or bottom of the cable compartment. A removable steel cable pull box (see Bus Compartment) is provided to isolate cables when two circuit breakers are installed in one vertical section.

Conduit should be stubbed in the concrete as part of the site preparation before the assembly is installed, but top entrance conduit must be installed after the assembly is in place. The top covers can be removed, punched to fit the conduit, and put back in place.

The front conduit area is for the bottom circuit breaker when all cables enter from below, and for the top circuit breaker when all cables enter from above. The cable pull box may be removed to install the rear cables first. The cable pull-box must be reinstalled to provide isolation. When required, zero-sequence current transformers (see Bus Compartment) are conveniently located in each cable compartment.

Various cable termination systems are used. These are detailed on the customer’s plans and specifications. Solderless or compression lugs (provided upon request) can be supplied on the load connectors. Tape and insulating material necessary for completing the field connection at the lug pad are not supplied with the assembly.

Schneider Electric provides lugs upon request. Tape and associated material for insulating cable terminations are not supplied.

Surge Arresters

Surge arresters are furnished only when listed in the user’s specifications. The vulnerability of the incoming and outgoing lines to lightning strikes or other high voltage transient conditions determines their type and justification. Surge arresters, when specified, are mounted in the incoming and outgoing cable compartments. Surge arresters must remain disconnected from the main bus during start-up testing. Surge arresters are shipped from the factory disconnected from the main bus to help prevent damage during hi-pot testing prior to energizing. Connect surge arrestors after hi-pot testing and before energization.

Circuit Breaker Product Overview

This section contains a basic overview of the workings of the Type VR, 27 kV circuit breaker designed for use with the Masterclad switchgear.

Circuit Breaker, Front View with Circuit Breaker Cover

Rating Nameplate

The rating nameplate is located on the front of the circuit breaker and shows the circuit breaker rating.

Indicators

The OPEN (O) / CLOSED (|) indicator (see Circuit Breaker, Front View with Circuit Breaker Cover) shows whether the vacuum interrupter contacts are OPEN (O) or CLOSED (|). The CHARGED/DISCHARGED indicator shows whether the closing springs are charged or discharged.

Circuit Breaker, Front View without Circuit Breaker Cover

Operating Mechanism

The operating mechanism is a stored energy-type mechanism. It uses spring assemblies to perform circuit breaker openings and closing functions.

Closing Spring Assembly

The closing spring assembly closes the circuit breaker when the CLOSE (|) pushbutton is pressed or when the close coil (see Trip and Close Coils) is energized. The spring assembly is charged (compressed) mechanically by the manual charging arm or electrically by the spring charging motor. When the control power is applied to the circuit breaker, the spring charging motor is energized. The charging motor turns the gear assembly which drives the ratchet assembly and compresses the closing spring assembly (see Left Side of Mechanism).

Opening Spring Assembly

The opening spring assembly opens the circuit breaker when the OPEN (O) pushbutton is pressed, or the opening coil is energized. The spring assembly is compressed whenever the circuit breaker is in the CLOSED (|) position.

Vacuum Interrupters

Vacuum interrupters are mounted vertically at the rear of the circuit breaker frame and perform the circuit breaker interruption.

Circuit Breaker, Side View

Primary Disconnects

The primary connection to the associated switchgear is through the six primary disconnects mounted horizontally at the rear of the circuit breaker.

NOTE: Never use the primary disconnects as handles when moving the circuit breaker.

Control Circuit

A typical schematic diagram for the control circuit of the Type VR circuit breaker is shown in Typical Control Circuit Schematic (Shown with Closing Spring Assembly Charged and Power OFF). The control circuit design may vary, depending upon customer requirements. Always refer to the specific schematic diagram for the specific Masterclad switchgear in question.

Typical Control Circuit Schematic (Shown with Closing Spring Assembly Charged and Power OFF)

Auxiliary Switch

The auxiliary switch (see Auxiliary Switch and Anti-Pump Relay) is a multi-stage switch used to operate circuits that depend on the position of the circuit breaker contacts. The schematic diagram in Typical Control Circuit Schematic (Shown with Closing Spring Assembly Charged and Power OFF) illustrates how each of the auxiliary switch contacts interconnect with the circuit breaker circuitry. The auxiliary switch functions as follows:

  • Two Type-a auxiliary contacts connect in series with the trip coil. Because these stages are OPEN (O) when the circuit breaker is in the OPEN (O) position, the auxiliary contacts de-energize the trip coil when the circuit breaker is in the OPEN (O) position.

  • The Type-b contact, connected in series with the closing coil, opens to de-energize the closing coil when the circuit breaker main contacts are in the CLOSED (|) position.

As shown, several Type-a and Type-b contacts are provided for optional use.

Auxiliary Switch and Anti-Pump Relay

Motor Limit Switch

The motor limit switch (see Motor Limit Switch) energizes the spring charging motor (see Circuit Breaker, Front View without Circuit Breaker Cover) when a closing spring charging operation is required. The motor limit switch de-energizes the spring charging motor when the closing springs reach the fully charged position.

As shown in the schematic diagram, the motor limit switch is connected to the motor in the normally OPEN (O) position. (see Typical Control Circuit Schematic (Shown with Closing Spring Assembly Charged and Power OFF)). When the closing springs are in the discharged position, the motor limit switch cam actuates the motor limit switch. This energizes the motor and disables the closing coil. Once the closing springs are fully charged, the cam allows the switch to assume the OPEN (O) position, de-energizing the spring charging motor.

Motor Limit Switch

Spring Charging Motor

When energized by the closing of the motor limit switch, the spring charging motor (see Left Side of Mechanism) drives the series of connected gears. These gears in turn raise and lower the ratchet assembly to compress the closing springs to the charged and latched position. When the closing springs are fully charged, the motor limit switch contacts reopen, de-energizing the spring charging motor.

Left Side of Mechanism

Latch Check Switch

The latch check switch indicates that the circuit breaker is ready for subsequent operation.

Anti-pump Relay

If the closing coil circuit is continuously energized, the anti-pump relay (see Auxiliary Switch and Anti-Pump Relay) helps ensure that the circuit breaker does not “pump” OPEN (O) and CLOSED (|) if a a trip signal is also present. The anti-pump relay performs this function by allowing the closing coil to activate only if:

  • The circuit is energized,
  • The closing springs are fully charged,
  • And the spring charging motor is de-energized.

The anti-pump relay activates when the close circuit is energized while the circuit breaker is closed. If the close circuit is energized continuously, the anti-pump relay remains in the energized position after the 52/a auxiliary contact closes during the closing operation. When the anti-pump relay is energized, a pair of its normally-closed contacts, in series with the close coil, open to help ensure that the close coil cannot be energized. The close coil activates only when the close circuit is de-energized (de-energizing the anti-pump relay), then energized again.

Trip and Close Coils

The standard location of the trip and close coils is in the upper center of the operating mechanism. When energized by the switchgear or remote circuitry, these coils release the open or close latches located inside the mechanism.

NOTE: Optional tripping and closing functions could require that these coils be located on the outside of the mechanism frame. To access the trip and close coils, unclip the mechanism cover from the mechanism frame.

Trip and Close Coils

Motor Cutoff Switch

The motor cutoff switch is located under the base of the Type VR circuit breaker. The motor cutoff switch de-energizes the spring charging motor circuit during the installation of the circuit breaker or its removal from the compartment.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.