6055-40 Rev. 02

Inspection and Maintenance

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462 or local equivalent.
  • Only qualified personnel familiar with medium voltage equipment are to perform work described in this set of instructions. Workers must understand the hazards involved in working with or near medium voltage circuits.
  • Perform such work only after reading and understanding all of the instructions contained in this bulletin.
  • Turn off all power supplying this equipment before working on it.
  • Always use a properly rated voltage sensing device to confirm that power is off.
  • Before performing maintenance on this device, disconnect all sources of electric power. Assume all circuits are live until they are completely de-energized, tested, grounded, and tagged. Pay particular attention to the design of the power system. Consider all sources of power. Check interconnection diagrams and make sure there are no backfeed potential sources.
  • Use out-of-service tags and padlocks when working on equipment. Leave tags in place until the work is completed and the equipment is ready to be put back into service.
  • Do not open a circuit breaker door unless the circuit breaker is open.


  • Never disconnect the main trip source of energized equipment.
  • Handle this equipment carefully and install, operate, and maintain it correctly so that it functions properly.
  • Be aware of potential hazards, wear personal protective equipment, and take adequate safety precautions.
  • Do not make any modifications to the equipment or operate the system with interlocks and safety barriers removed. Contact your local Schneider Electric representative for additional instructions if the equipment does not function as described in this manual.
  • The complete assembly arrangement determines if the top or bottom contacts are the line side; both can be energized when the circuit breaker is removed from the compartment. Identify the line side contacts for each circuit breaker compartment.
  • Disconnect all high voltage to the switchgear before accessing the horizontal bus compartment.
  • Carefully inspect your work area and remove any tools and objects left inside the equipment before energizing the switchgear.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, or Arc Flash
  • Replace all devices, doors, and covers before connecting the power to this equipment.
  • All instructions in this manual are written with assumption that the customer has taken these measures before performing maintenance or testing.
Failure to follow these instructions will result in death or serious injury.

Cleaning Instructions

This equipment contains components manufactured with various materials. Some cleaning agents could damage the integrity of the surface of the component reducing its insulating properties, structural strength or conductivity. Use this guide to determine a compatible cleaning agent for typical materials incorporated in this equipment. Never spray cleaners or use compressed air on or inside the equipment as this will cause the contamination or cleaners to become airborne and could contaminate other components.

  • Greased joints:

    • Wipe surface grease away with a clean cloth. Reapply the grease recommended for that assembly, found in the maintenance section of the documentation for that assembly.

  • Glass polyester insulator surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use distilled or purified water to moisten the cloth in place of denatured alcohol, but standing/pooling water must be absorbed and not left to air dry.

    • Use care so the liquid does not flow between bus joints.

  • Epoxy insulator surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use distilled or purified water to moisten the cloth in place of denatured alcohol, but standing/pooling water must be absorbed and not left to air dry.

    • Remove residue by lightly rubbing with a dry Scotch-Brite non-scratch scour pad followed by wiping with a clean cloth moistened with denatured alcohol, distilled or purified water.

    • Use care so the liquid does not flow between bus joints or between the epoxy coating and bus.

  • Ceramic/porcelain insulator surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use distilled or purified water to moisten the cloth in place of denatured alcohol, but standing/pooling water must be absorbed and not left to air dry.

    • Use care so the liquid does not flow between bus joints or between the epoxy coating and bus.

    • Remove residue by lightly rubbing with a multi-functional HV insulator cleaning paste on a clean cloth followed by wiping with a clean cloth moistened with denatured alcohol, or distilled or purified water.

  • Poly concrete standoff insulator surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use care so the liquid does not flow between bus joints.

  • Plastisol boot surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use distilled or purified water to moisten the cloth in place of denatured alcohol, but standing/pooling water must be absorbed and not left to air dry.

    • Use care so the liquid does not flow inside the boot and between the bus joints.

  • Polycarbonate/Lexan surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use distilled or purified water to moisten the cloth in place of denatured alcohol, but standing/pooling water must be absorbed and not left to air dry.

    • Do not wipe in a circular motion, use linear strokes directed toward an exposed edge.

    • Change the water and rinse the cloth often.

    • Dry with a clean cloth.

    • Use denatured alcohol dampened on a clean cloth on the polycarbonate/Lexan insulation barriers as there is no UV protection applied to the sheet that would cause degradation.

  • Silver/tin plated copper surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Remove residue by lightly rubbing with a dry Scotch-Brite non-scratch scour pad followed by wiping with a clean cloth moistened with denatured alcohol.

    • Use care so the liquid does not flow between bus joints.

  • Powder coated surfaces:

    • Wipe with a clean cloth dampened with denatured alcohol.

    • Use distilled or purified water to moisten the cloth in place of denatured alcohol, but standing/pooling water must be absorbed and not left to air dry.

    • Remove residue by lightly rubbing with a dry Scotch-Brite non-scratch scour pad followed by wiping with a clean cloth moistened with denatured alcohol, or distilled or purified water.

    • Use care so the liquid does not splash or flow into seams or onto other components.

  • Control component surfaces:

    • Low voltage wires within this equipment are SIS insulated and may be wiped with a clean cloth dampened with distilled or purified water. Do not use alcohol.

    • Circuit boards can have isopropyl alcohol applied by small brush to remove deposits.

    • Solvents and alcohol (denatured, isopropyl) can damage some plastics, such as amorphous plastics. When in doubt, use a clean dry cloth, or a clean cloth dampened with distilled or purified water and dry completely.

  • NOTES:

    • Do not use cleaners such as Lectra-Clean™ made by CRC (noted in some of the low voltage equipment manuals). Lectra-Clean can damage some plastics and other components.

    • Do not use chemicals such as Simple Green™ as it can cause corrosion on some parts and in some cases those cleaners describe rinsing the surface after application.

    • Do not splash or spray liquids as they can infiltrate areas that cannot be cleaned or dried properly.

    • Components within the equipment are not rated to be exposed to moisture. Exposure to moisture may cause performance issues to develop over the life of the product.

Main Bus Compartment

  1. Turn off all power supplying this equipment. Be sure there is no backfeed through any feeder circuit. Always use a properly rated voltage sensing device to confirm that power is off.

  2. Ground the main and feeder circuits.

  3. Disconnect and remove fuses.

  4. Disconnect and remove the circuit breaker.

  5. Remove the front and rear covers from each main bus compartment. Inspect the busbars, primary contact supports, and insulating barrier(s).

  6. Remove the insulating boots from the bus joints. Check all busbar connections and torque all 1/2 inch bolts to 55 lb-ft. (74.28 N•m).

    NOTE: Slight discolorations or tarnish of the silver plate is normal. Severe discoloration of the silver plate is an indication of an improper or loose contact and overheating. Clean the discoloration from the contact surfaces of the busbar and primary contact. Use an abrasive pad such as Scotch Brite.
  7. Vacuum each compartment to remove dust, spiderwebs, and others. Wipe off the insulation with a clean cloth.

  8. Lightly lubricate the moving primary and secondary contacts and fingers with Mobil 28 red grease, SquareD part number 1615-100950T.

  9. Lubricate all rollers and sliding parts with Mobil 28 red grease, SquareD part number 1615-100950T.

Replacing the Fuses

To replace damaged fuses in the VT drawout unit or CPT fuse drawout units:

NOTE: When replacing fuses, handle them carefully to avoid breakage. Do not grasp the fuse in the middle. Replace all fuses even if only one is damaged.
  1. Follow the procedures outlined in either Voltage Transformer (VT) Drawout Unit Inspection or Control Power Transformer (CPT) Primary Fuse Drawout Unit Inspection to withdraw the appropriate fuse drawout unit.

  2. Wearing personal protective equipment, such as insulated gloves and a face shield, grasp the fuse near the fuse clip and pull while rotating the fuse.

  3. Insert the fuses one end at a time into the fuse clips.

  4. Follow the racking procedures outlined in either Voltage Transformer (VT) Drawout Unit Inspection or Control Power Transformer (CPT) Primary Fuse Drawout Unit Inspection to return the unit to the CONNECTED position.

Re-Energizing

Install all of the circuit breakers to the TEST/DISCONNECT position with their secondary disconnects engaged:

  1. Remove the ground from the main and feeder circuits

  2. Close the compartment doors.

  3. Connect the control power source.

  4. Close the main source of power and operate each circuit breaker electrically in the TEST/DISCONNECTED position.

  5. If all controls are functioning properly, disconnect the secondary control plugs.

  6. Rack the circuit breakers into the CONNECTED position.

  7. Close the circuit breakers and resume normal operation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.