6055-40 Rev. 02

Accessories

MasterClad Lift Truck

One circuit breaker lift truck is required for each:

  • Two-high line up.

  • Switchgear installed on concrete pads that do not extend beyond the front of the switchgear.

  • NEMA 3R outdoor nonwalk-in switchgear.

The cradle is raised and lowered by a self-braking worm and pinion drive system with a winch and wire cable. No ratchet release or locking is required because of the automatic load-retaining clutch feature. Rotating the handle clockwise raises the cradle. Rotating the handle counterclockwise lowers the cradle.

Follow the instructions provided with the Masterclad lift truck to remove a circuit breaker from the circuit breaker compartment with the lift truck.

Masterclad Lift Truck

Test Cabinet (Optional)

An optional wall-mounted test cabinet (see Wall-Mounted Test Cabinet (Optional)) is furnished when listed in the user’s specifications. The test cabinet consists of a small enclosure with:

  • A power on-off toggle switch,

  • a white light indicating the power is on,

  • A red light indicating the circuit breaker is closed,

  • A green light indicating the circuit breaker is open,

  • Close and open pushbuttons, and

  • An eight ft. (2440 mm) cable with a secondary control receptacle that can be plugged directly into the circuit breaker control plug.

Refer to the customer drawings for the external power connections and requirements necessary for the cabinet. A convenient terminal block is provided inside the test cabinet for these connections.

Wall-Mounted Test Cabinet (Optional)

Ground and Test Devices

Two types of ground and test devices are available: manual and electrical. Ground and test devices are typically used for:

  • Grounding of circuits during maintenance periods and

  • Connection points for applying voltage for hi-pot testing and cable testing access to both line side and load side circuits for phase sequence testing.

NOTE: A complete description, operating instructions, and maintenance information are included in a separate ground and test devices instruction bulletin.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.