Conditions for Engaging the ERMS Function
The Energy Reducing Maintenance Setting (ERMS) function is available when the Energy Reducing Maintenance Settings Digital Module is purchased and installed on the Micrologic X control unit.
Energy Reducing Maintenance Setting (ERMS) Function Operating Principles
The ERMS function can be engaged with both the Masterpact MTZ Mobile App (password-protected) and an external selector switch.
The ERMS function must be disengaged by the interface that engaged it:
-
If it is engaged on a smartphone, it must be disengaged by the same smartphone.
-
If it is engaged by the external ERMS switch connected to the ESM module, it must be disengaged by the ERMS switch.
-
If it is engaged by both a smartphone and the ERMS switch, it must be disengaged by both that smartphone and the ERMS switch.
For more information, refer to the Micrologic X - Control Unit - User Guide (see Related Documents).
Engaging the ERMS Function
| NOTICE |
|---|
|
HAZARD OF LOSS OF POWER
Confirm that the Energy Reducing Maintenance Setting (ERMS)
protection settings are properly configured prior to engagement.
Failure to follow these instructions can result in loss
of service due to power loss.
|
The ERMS can be engaged in different ways, according to the device configuration and its accessories:
|
Type |
Accessories |
Action |
|---|---|---|
|
Through Masterpact MTZ Mobile App |
— |
Send a command from the Masterpact MTZ Mobile App to engage the ERMS function, through Bluetooth wireless communication or USB OTG connection. The action is password-protected. |
|
Through an external selector switch connected to the ESM module |
|
Turn the external selector switch to the Engaged position |
Disengaging the Energy Reducing Maintenance Setting (ERMS) Function
DANGER |
|---|
|
HAZARD OF ELECTRICAL SHOCK, EXPLOSION, OR ARC FLASH
Prior to disengaging the Energy Reducing Maintenance Setting
(ERMS) function:
Failure to follow these instructions will result in death or serious injury.
|
A digital lock function establishes a digital lock between a smartphone running the Masterpact MTZ Mobile App and the Micrologic X control unit when ERMS is engaged by the smartphone. The digital lock function ensures that when the ERMS function is engaged by a smartphone, it must be disengaged by the same smartphone.
The way to disengage the ERMS function depends on how it was engaged:
|
Type |
Accessories |
Action |
|---|---|---|
|
Through Masterpact MTZ Mobile App |
— |
Disengage the ERMS function on the same smartphone that engaged it |
|
Through an external selector switch |
|
Turn the external selector switch to the Disengaged position |
|
Through Masterpact MTZ Mobile App and an external selector switch |
|
|
DANGER