0614IB1702

Diagnosing Masterpact X Error Messages

The following table shows the sequence of actions to take after an error message is received from the Micrologic X control unit. Further explanation of each action is given in the following paragraphs.

Stage

Description

1

Identify the problem detected.

2

Acknowledge the cause on the Micrologic X display screen.

3

Consult the list of error messages and perform the recommended actions.

Identify the Problem

An error message is displayed when the Micrologic X control unit detects an internal problem.

Example of error message:

Acknowledging the Error Message

Acknowledge the error message on the Micrologic X control unit display screen.

Step

Action

1

Consult the list of error messages in the following tables and perform the actions recommended.

2

Press OK to acknowledge the message and return to the Home menu.

3

Press the Test/Reset button for 3 seconds to reset the control unit.

Action after Receiving Error Message

Recommended action after receiving a Micrologic X control unit error message.

Code

Error Message

Description

Recommended Action

1 to 24
157
190

Service not performed - internal problem

The requested action was not performed due to an internal problem.

Repeat the action that caused the error message. If the message is displayed again, switch off the 24 Vdc of the Micrologic X control unit and switch it on again. If the problem persists, call Schneider Electric field service.

158

Command rejected, already in progress

The Micrologic X control unit has detected simultaneous orders (for example between IO and control unit).

Repeat the command.

169

Command rejected, already in asked state.

The Micrologic X control unit is already in the requested state.

Check that the Micrologic X control unit is in the required state. If it is not, repeat the command.

174

Session Key is invalid

The request action was not performed because the session key is not valid.

Repeat the action that caused the error message. If the message is displayed again, switch off the 24 Vdc of the Micrologic X control unit and switch it on again. If the problem persists, call Schneider Electric field service.

175

Out of session scope

The requested action was not performed because it is not within the session scope.

Repeat the action that caused the error message. If the message is displayed again, switch off the 24 Vdc of the Micrologic X control unit and switch it on again. If the problem persists, call Schneider Electric field service.

176

Session is already opened

The Micrologic X control unit has detected simultaneous settings sessions (for example, Ecoreach and control unit).

Press OK to clear the message and then repeat the command.

177

No session is open

Submit/apply operations have not been performed within five minutes.

Start a new session, re-enter the settings, then submit and apply them.

180

Bluetooth disabled! To enable go to Configuration menu.

Bluetooth communication has not been enabled for the Micrologic X control unit.

Enable Bluetooth communication from the Micrologic X control unit menu > Configuration > Communication > Bluetooth.

Contact a Schneider Electric field service representative for more information about who can carry out the recommended actions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?