0614IB1702

Micrologic X Control Unit Description

The Micrologic X control unit includes:

  • Micrologic X status LEDs.

  • A local HMI comprising a graphic display with colored backlight, contextual buttons, and dedicated buttons.

  • LEDs to monitor circuit breaker operations as well as the source of trips and alarms.

Control Unit Layout

  1. Ready LED

  2. Service LED

  3. ERMS LED

  4. HMI display screen

  5. Escape button ESC

  6. Three contextual buttons

  7. Home button

  8. NFC wireless communication zone

  9. Bluetooth LED

  10. Bluetooth activation button

  11. Test button for ground-fault protection (Micrologic 6.0 X)

  12. Test/Reset button for trip cause LEDs and alarms

  13. Mini USB port under rubber cover

  14. Overload and trip cause LEDs

  15. Cover for internal battery

  16. Voltage power supply module (VPS) (optional)

  17. VPS LED to indicate that the VPS is supplying the control unit

  18. QR code for product information

  19. Control unit identification number

  20. Control unit type

  21. Sensor plug with the rated current of the circuit breaker

  22. Plastic cover

Micrologic X Status LEDs

LED

Description

Ready

The Ready LED flashes when the control unit is ready to provide standard protection.

The service LED indicates the overall health of the circuit breaker:

  • Unlit LED: the circuit breaker is in good working order

  • Orange LED: non-urgent alert message

  • Red LED: alert message that requires immediate action

ERMS

The ERMS (Energy Reduction Maintenance Setting) LED has the following statuses:.

  • Blue LED: ERMS engaged

  • Off LED: ERMS disengaged

Local HMI Display Screen with Contextual and Dedicated Buttons

Use the local HMI screen and buttons to:

  • Navigate the menu structure

  • Display monitored values

  • Access and edit configuration settings

NFC Communication Zone

Use the NFC communication zone to create an NFC connection between a smartphone running the Masterpact MTZ Mobile App and the Micrologic X control unit. When the connection is established, the circuit breaker operating data is automatically uploaded to the smartphone.

Bluetooth Activation Button and LED

Use the Bluetooth activation button to create a Bluetooth low-energy connection between a smartphone running the Masterpact MTZ Mobile App and the Micrologic X control unit. When the connection is established, the circuit breaker can be monitored and controlled from the smartphone.

The Bluetooth LED blinking indicates that a Bluetooth device is in communication.

Micrologic X Control Unit Test Button

Use the test button to test the ground-fault protection for Micrologic 6.0 X control units.

Micrologic X Control Unit Test/Reset Button

The Test/Reset button performs the following functions:

  • Test internal battery or check LED functionality: press and hold the Test/Reset button for less than three seconds, the four trip cause LEDs switch off for one second. One of the following results:

    • The four trip cause LEDs switch on for two seconds: the battery is OK.

    • The four trip cause LEDs flash sequentially for two seconds: the battery is near the end of its life. Replace the battery.

    • The four trip cause LEDs do not light: replace the battery.

  • Reset: press and hold the Test/Reset button for more than three seconds to reset the control unit. The trip cause LEDs and the service LED switch off.

NOTE: When the Micrologic X control unit is not powered by an external 24 Vdc power supply or through a USB connection, the Micrologic X control unit can be restarted by pressing and holding the Test/Reset button for 15 seconds. The standard protection functions remain active during the restart.

Micrologic X Control Unit Mini USB Port

Remove the rubber cover of the mini USB port to connect the following devices:

  • A Mobile Power Pack to supply power to the Micrologic X control unit.

  • A smartphone running the Masterpact MTZ Mobile App through USB OTG connection.

  • A PC equipped with Ecoreach software.

NOTE: The Micrologic X control unit does not support USB keys. Even if a USB key is connected using an adaptor, data is not transferred.

Micrologic X Control Unit Overload and Trip Cause LEDs

The indications of the four trip cause LEDs depend on the type of control unit.

LEDs

Description

Micrologic 3.0 X, 5.0 X, 6.0 X: Overload pre-alarm, the load exceeds 90% and is lower than 105% of the Ir setting of the long-time protection.

Micrologic 3.0 X, 5.0 X, 6.0 X: Overload alarm, the load exceeds 105% of the Ir setting of the long-time protection.

Micrologic 3.0 X, 5.0 X, 6.0 X: Trip due to long-time protection.

Micrologic 3.0 X: Trip due to instantaneous protection.

Micrologic 5.0 X, 6.0 X: Trip due to short-time protection or instantaneous protection.

Micrologic 3.0 X, 5.0 X: Not used.
Micrologic 6.0 X: Trip due to ground-fault protection.

Micrologic 3.0 X, 5.0 X, 6.0 X: Trip due to other protection (optional protections activated via digital modules).

Micrologic 3.0 X, 5.0 X, 6.0 X: Invalid Micrologic control unit self-test

NOTE: If the Micrologic X control unit is not powered, the trip cause LEDs go off after four hours. After this period, press the Test/Reset button to light them again.

Micrologic X Internal Battery

The internal battery powers the trip cause LEDs and the main diagnostic functions in the absence of any other power supply.

Micrologic X VPS Voltage Power Supply Module

The optional VPS power supply module provides an internal voltage supply to the Micrologic X control unit.

Micrologic Control Unit QR Code

When the QR code on the front face of a Micrologic X control unit is read with a smartphone running a QR code reader and connected to the internet, the Go2SE landing page is displayed (seeGo2SE Landing Page). The landing page displays information about the device and a list of menus.

Micrologic X Control Unit Identification Number

The identification number consists of:

  • The serial number of the Micrologic X control unit in the format FFFFFFYYWWDXXXXX.

  • The commercial reference of the control unit in the format LV8XXXX.

Use the identification number to register the Micrologic X control unit.

Registering the Micrologic X control unit enables up-to-date record keeping and traceability.

Micrologic X Control Unit Type

This code indicates the type of Micrologic control unit:

  • The number (for example, 3.0) defines the types of protection provided by the control unit.

  • The letter (X) identifies the range.

Micrologic X Sensor Plug

The protection ranges depend on the rated current In, defined by the sensor plug present below the Micrologic X control unit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.