Masterpact MTZ—Extreme Atmospheric Condition
Masterpact MTZ devices have successfully passed tests for extreme atmospheric conditions, defined by the following standards:
Standard |
Title |
---|---|
IEC 60068-2-1 |
Dry cold, at -40°C (-40°F) |
IEC 60068-2-2 |
Dry heat, at +85°C (+185°F) |
IEC 60068-2-30 |
Damp heat (temperature +55°C (+131°F), relative humidity 95%) |
IEC 60068-2-52 level 2 |
Salt mist |